This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61165: TPS61165

Part Number: TPS61165
Other Parts Discussed in Thread: TPS92390

the device TEXAS TPS61165DBVR do no work properly with LOW PWM level (4%), the current output goes up from 1mA up to 4mA without reasons. The problems seems to be link with the input voltage, when the input voltage changes from 12V to 14,5V the output current goes up. This problem seems to be and instability on the feedback control loop, please look at the attached document.