Dear customer support staff,
The data sheet has the following description, and so is Figure 7.
"The LED current setting can be in the range of 0.5A up to 2A maximum."
I would like to set the current to a maximum of 0.2A. Is it possible?
When the maximum current is 200mA, the resistance value will be calculated to be 123.75kohm (24.75 / 0.2).
It can be set, but does it mean that the current variation will be large?
Best regards,
Nakayama