This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
For lm25118, there are two mode, buck and buck-boost. In what condition it will shift from buck to buck -boost? Does it related to the load current?
In the datasheet, it simply explain that it will shift to buck-boost when D = 75%
In a circuit where Vout should be12V/3A , when Vin = 15V , the output is about 10.8V/3A (stability with load ), the HO duty cycle is about 80%; Lo is low , and the Rt=12k; the Vout will decrease from 12V/3A to10.8V/3A when Vin from 18V down to 14V. What's the reason for that?
Thanks a lot.
Matthew Chen
Hi Stefan,
1. From the datasheet, I see when the duty circle of Buck reaches to 75%, than the boost duty circle begins to increase, is D(buck)>75% the only requirement for the chip to shift to buck-boost? If not, what are the detail conditions that the chip will shift from Buck to Buck-mode?
2. In figure, it's obviously that the shift point of the Duty is much higher the 75%, what the reason for that?
Thanks a lot
Matthew Chen
HI Matthew,
as this is not a parameter from the parameter section this is not be specified accurately.
So you might read the text more that way: Once the duty cycle reaches ~ 75%, the ...
From the graph above i would say this was 78% for that specific device which was used for the measurement.
But as this is depending on Device, Temperature, .... this can also shift.
Best regards,
Stefan
Hi Matthew,
I have not seen an update on this thread for the last 15 days.
If the issue is solved it would be great to press the is solved button.
If there is still something open, just let me know with the new details.
Best regards,
Stefan