This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi experts,
This is Koki Tsushima,
Customer wants to know efficiency curve when 5V output like this.
Is it possible to share with me?
I guess customer wants to use this by 1LiPo so Vin =3~4.5V.
Iout is few mA~ up to 10mA.
Best,
Koki Tsushima
Hi Koki-san,
Sorry that we don't have 5V output efficiency curve because the validation only tested 18V output before. I can test the efficiency based on EVM at customer's required application such as 3.6V input, 5V output, 10mA load. But because of quarantine policy due to COVID, I cannot return to office in short time. Maybe customer can apply for one EVM to evaluate themselves or I can test the efficiency after return to office 10 days later.
BR
Eric Yue
Hi Eric-san,
Thank you for your continuous support.
Is it possible to measure now?
BR,
Koki Tsushima
Hi Koki-san,
As you may know, the COVID situation in shanghai is worse now. I cannot return to office for at least one week. I will test it as soon as I return. Please help get us some more time because of this irresistible factors. Thanks.
BR
Eric Yue