This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Good Day. I have a customer who is working with TPS73601DRBT/R. Please see below his query for your reference. Thank you very much.
We currently have a CCA that is set up to use the TPS73601DRBT/R part due to supply chain issues, I am trying to find a drop in replacement
We have 3.3V input, and need 1.8V outputs (at least 400mA output current), TPS73701DRBT/R and TPS73501DRBT/R are the 2 candidates that we are looking at.
Was hoping to get some guidance on whether these are suitable drop in replacements, whether there are any design concerns, or whether there are any other better candidates with better stock/lead times.
Best Regards,
Ray Vincent
Hey Ray,
I think both of these are good chooses, I would recommend the TPS737 as it is a closer match. Just be aware of the differences between devices, neither of the other devices are stable without caps, as well as different accuracy and dropout rating.
Hope this is helpful!
Thanks,
McKyla