This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS736: cheaper alternative to TPS73601DRBT

Part Number: TPS736
Other Parts Discussed in Thread: TPS746, TPS745, TLV757P, TLV755P

Hello team,

my customer has been using the TPS73601DRBT for a long time in order to power a Vcore physical Ethernet. Now they are redesigning the same family of product by introducing an entry level and they wanted to change the TPS73601DRBT for a lower cost version.

Specs are 1.2V@400mA or even higher current but they could live with 400mA; the solution that I'm looking for can be an LDO or step-down.

Could you please let me know if you have any recommendation?

Thank you and best regards,

Adrian

  • Hi Adrian,

    Please consider our new TPS745 which is rated for up to 500mA, or its sister device TPS746 which is rated up to 1A.

    If fixed devices are needed please consider our TLV755P and TLV757P family.

    Regards,
    Wilson