Part Number: UCD90910
Hi
Your technical department has confirmed the Fan drive 'FPWM' outputs are limited to 3v3 due to the internal protection diodes.
Just to mention - the data sheet is a bit misleading as it shows a direct PWM fan drive from the IC to the 12V fan PWM input.
I now have to add 2 transistors to the output drive of each of the 10 fans.
Two transistors are needed to ensure the signal is not inverted.
Instead of the transistor PWM drive can I use a series resistor to reduce the voltage back into the IC.
I have included an image of the Fan PWM input and the transistor drive circuit I have initially used.