This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Normally I would take the time to review the DS to help answer this Q, but I am currently resource-strained.
I need to know a summary of all the ways PGOOD works.
1) How the Output Voltage and PGOOD (I am 100% sure this is in the DS)
2) How the EN pin voltage and PGOOD work
Any other ways PGOOD could be triggered High/Low
(Overcurrent, etc)
Regards,
Darren
Hi Darren,
The PG pin is an open-drain output that requires a pull-up resistor to any voltage up to a voltage level of the input voltage at VIN. It can sink 2 mA of current and maintain
its specified logic low level.
When EN=HI and PG > VTH_PG then PG is high. When EN=HI and PG < VTH_PG then PG is low. PG is low when the device is turned off due to EN, UVLO or thermal shutdown. VIN must remain present (>0.7V) for the PG pin to stay low.
Here is the table summary:
VTH_PG thresholds are mention in EC table:
Hope this helps.
Thanks,
Amod