Other Parts Discussed in Thread: BQ25792
With a single cell configuration, I am using a 5V/3A adaptor on VAC1 input but cannot get the BQ to charge the cell even though it reports it is charging (STAT LED on and ADC control reg 0x2E bit 7 set to 1). IBAT current remains reported as 0mA, yet an inline amp meter (with the battery), shows a constant _drain_ of about 160mA.
I did not hot-swap the battery nor inadvertently reversed the leads to it. Just started working with this chip a few days ago - seems overly complicated or I am making some dumb mistakes here. Help appreciated.
BQ25792 dump
Register Hex Binary
REG 00 : 0x0C 00001100b
REG 01 : 0x01A4 0000000110100100b
REG 03 : 0x00C8 0000000011001000b
REG 05 : 0x2D 00101101b
REG 06 : 0x008F 0000000010001111b
REG 07 : 0x8F 10001111b
REG 09 : 0x05 00000101b
REG 0A : 0x23 00100011b
REG 0B : 0x00DC 0000000011011100b
REG 0D : 0x4B3D 0100101100111101b
REG 0E : 0x3D 00111101b
REG 0F : 0xA2 10100010b
REG 10 : 0x80 10000000b
REG 11 : 0x40 01000000b
REG 12 : 0x00 00000000b
REG 13 : 0x41 01000001b
REG 14 : 0x96 10010110b
REG 16 : 0xC0 11000000b
REG 17 : 0x7A 01111010b
REG 18 : 0x54 01010100b
REG 19 : 0x008F 0000000010001111b
REG 1B : 0x0B 00001011b
REG 1C : 0x6A 01101010b
REG 1D : 0x01 00000001b
REG 1E : 0x50 01010000b
REG 1F : 0x00 00000000b
REG 20 : 0x00 00000000b
REG 21 : 0x00 00000000b
REG 22 : 0x00 00000000b
REG 23 : 0x00 00000000b
REG 24 : 0x00 00000000b
REG 25 : 0x00 00000000b
REG 26 : 0x00 00000000b
REG 27 : 0x00 00000000b
REG 28 : 0x00 00000000b
REG 29 : 0x00 00000000b
REG 2A : 0x00 00000000b
REG 2B : 0x00 00000000b
REG 2C : 0x00 00000000b
REG 2D : 0x00 00000000b
REG 2E : 0x80 10000000b
REG 2F : 0x00 00000000b
REG 30 : 0x00 00000000b
REG 31 : 0x0000 0000000000000000b
REG 33 : 0x0000 0000000000000000b
REG 35 : 0x1508 0001010100001000b
REG 37 : 0x1502 0001010100000010b
REG 39 : 0x0000 0000000000000000b
REG 3B : 0x0FD2 0000111111010010b
REG 3D : 0x0F96 0000111110010110b
REG 3F : 0x0253 0000001001010011b
REG 41 : 0x003C 0000000000111100b
REG 43 : 0x0000 0000000000000000b
REG 45 : 0x0000 0000000000000000b
REG 47 : 0x00 00000000b
REG 48 : 0x08 00001000bvbat 0x0FC0 :4032 mV
ibat 0x0000 :0 mA
vbus 0x1511 :5393 mV
ibus 0x0000 :0 mA
vsys 0x0F8E :3982 mV
vac1 0x150E :5390 mV
vac2 0x0000 :0 mV