This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5450: Back feeding the regulator in shutdown

Part Number: TPS5450


I have a TPS5450 that regulates 14V from a 24V input. When input power fails, the TPS5450 shutdown pin is pulled low. As the 14V output decays, a power path FET switches to a 9V battery to feed the downstream system. However, the battery will also put voltage on the PH pin (through the inductor).

Will this cause any internal issues?