This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
My customer is looking for a buck-boost converter that can be used with the following conditions.
- Input : 15V ~ 9V (SMPS 15V or Battery 9V ~ 14.2V)
- Output : 12V / 5A
Could you please recommend a suitable device?
Thank you.
JH
Hi JH,
thank you for using the E2E forum.
A good starting point for this are always the available reference designs:
Best regards,
Stefan