Hello,
looking at data sheet of BQ76952 I read that TS2 as input port can tolerate an input voltage between 0V - 2V (corresponding to VREG18), when used as ADC input pin. No mention about other case/use.
- Consider TS2 pin not used for thermistor measurements: it is possible in RUN mode to connect TS2 pin to a 3.3V by means of an external pull up resistor?
- Consider TS2 pin not used for thermistor measurements: It is possible in RUN mode to change the volage level (high->Low->high->Low->..) of the TS2 pin or this is a problem?
- Consider using the SHUTDOWN mode of BQ76952: In order to strengthen the output of the TS2 pin in shutdown mode, is it possible to add an external 5V pull up or a weak current source (2uA-3uA) on TS2 pin?
Thanks in advance
Francesco