Other Parts Discussed in Thread: LM10011, INA226,
Hi TI Team,
We have completed design using TPS543C20 in dual phase stacked configuration. The LM10011 current DAC is used in 6 bit mode to vary the output voltage in the range of 0.686V to 0.926V by keeping nominal value at 0.8V for 30.1uA current, RSET = 118K. An ADC with P/N INA226 is used to measure voltage, current and power at the load side. The DAC and ADC are connected to a controller board. The measured value from ADC will be checked by the controller board and the DAC current will be varied accordingly.
We would like to perform simulation by including all these 3 components to check the working of TPS543C20 and its output characteristics while varying and measuring the output.
1. Which tool is suitable to perform this simulation.?
2. Does TI provide support by performing simulation.? If yes what and all inputs we need to provide to do same.?
Thanks & Regards,
Vyshnav Krishnan