Other Parts Discussed in Thread: TPS3703, TPS3702, TPS3704
There are 4 graphs in datasheet regarding sense glitch immunity (figure 7-11 to 7-14). Furthermore there are typical values in table in section 7.6. Unfortunately the values do not fit together. Section 7.6 states 3.5us for 5% overdrive at Vdd=3.3V (undervoltage/ overvoltage) If I am looking into the graphs 7-11 to 7-14 for Vdd=1.7 and 5.5V respectively the values are all higher:
12.5 to 15.5 us @ Vdd = 1.7 V and
7.5 to 8 us @ Vdd = 5.5 V
In our case Vdd=3.3V and my assumption is that I can simply interpolate the values from 5.5V and 1.7V to the desired Vdd=3.3V. Either the values in the section 7.6 are wrong or the interpolation does not work or cannot be applied. In the latter case I kindly ask to provide the graphs for Vdd=3.3V. We need the graphs for worst case calculations.