Hi,
I am wanting to design a boost converter with:
Vin = 24V
Iin = 25A max
Vout = 120V
Iout = 4A
I am looking at using the LM5156 but I have noticed the maximum Vcc is 16V. I was thinking to use a voltage divider to solve this problem. I also wanted to know if the LM5156 was suitable for stepping the voltage up to 120V or do I need to be looking at another IC?
Kind regards
Jacob