This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27710: digtial IO

Part Number: UCC27710

Hi,

I have to design an 24V digital output which must be configurable by a uC to be either a high side 24V switch or a low side 24 V switch. Therefore the question is, is it possible to use a half bridge for designing it. When the configuration is a low side switch only the low side FET should be switched on/off. In my opinion this should be no Problem. When it is configured as a high side 24 V output, the high side switch should only be switched on and off. I think here could the boostraping a problem.

If a half bridge is not the right device, can please advise me a different product from your portfolio.

I hope I have described it in a understandable way.

Thank you for you support

Thanks Michael