Hello TI Team,
I have done the schematic design of TPS546C23 buck- regulator with the below requirement. I want to control output from PMBus and Hardware.
1. 1.3V@10-13A , O/P ripple= 10mV Vp-p, Voltage tolerance= 1%
2. 3.3V@22-27A, O/P ripple= 9mV Vp-p, Voltage tolerance= 5%


Can someone review it and provide the valuable inputs by generation the o/p with both the option?