Hi
The customer test with BQ76952, they found that when disconnect the C/DMOS during discharge will cause the BQ76952 unable to collect the cell voltage.
They read the battery status register and found that the POR is set. As long as the chip is restarted, it will return to normal.
This phenomenon only occurs when the MOS is disconnected in the discharge state, and it will not occur when the MOS is disconnected in the charge state.
Why the BQ76952 will POR when disconnect the MOS during discharge.
Thanks
Star