Other Parts Discussed in Thread: TINA-TI, LM2990
Hi Team,
Our customer is considering the LM25088 for audio electronics application with the following specifications.
Vin: 12V to 15V
Vout: -12V
Iout min: 10mA
Iout max: 1.1A
The design will power audio electronics, so switching frequency should be at 400khz min.
Webench generated the design file below.
https://webench.ti.com/power-designer/switching-regulator/customize/170
According to our customer, he downloaded a TINA ref design from our website and modify it per the circuit in the Webench but for some reason it doesn't seems to work. Please see the TINA-TI file from our customer.
He also added,
Regards,
Danilo