This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
My customer is studying every PROCHOT behavior of BQ24780S is latch or just a pulse. Also, there are 2 questions as below:
1. According to datasheet, will PROCHOT behavior of ACOK and BATPRES are latch or pull low pulse? Could you please help to clear what is mean one-shot
2. My customer test the PROCHOT behavior of ACOK and BATPRES and found PROCHOT was latched. But I reproduced condition on EVM and found the PROCHOT behavior was a pull low pulse.
Could you please comment about customer's waveform? Thanks.
Test method:
a. AC+DC
b. remove AC ADP
c. ACOK will be latch till 0x3CH) bit2=0
Charge setting as below.
0x3C 0x9A56H
0x3D 0x7739H
Best regards,
Hardy
When any event in PROCHOT profile is triggered, PROCHOT is asserted low for minimum 10 ms (default
REG0x3C[4:3]=10). At the end of the 10 ms, if the PROCHOT event is still active, the pulse gets extended.
One shot means one minimum 10ms pulse.