This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3429: efficiency 80% and low on frequency more than 300khz

Part Number: LM3429

I have I problem with over temperature  LM3429 and switching MOSFET and system work with efficiency above 80%. Maximal efficiency is only on 300khz (Rt=82k) on more high frequency,  efficiency is very low.

Topology: buck-boost

Vin: 36V

Iout: 0.23A

MOSFET: Sir696DP

Inductor: CDRH127/LDNP-680MC SUMIDA 2.6A

schematic:

topology:

termal zones:

board: