This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5121-Q1: LM5121 efficiency improvement

Part Number: LM5121-Q1


We had assemble the board and tested with upto 10A. Initially we got efficiency less than 90%. After the removal of snubber circuit parallel to high side N channel MOSFET, we got efficiency upto 93%. Is there any method such that we can increase the efficiency further.

We need efficiency near to 96%