I am pretty new with Hot Pluggable Machine.
My current project is to create design that can plug and unplug the system at runtime.
The Machine consists of:
- DC Converter 1000 Watt with 800 uF capacitance
- DC Converter 200 Watt with 1300 uF capacitance
- DC Converter 50 Watt with 300 uF capacitance
3 of the DC Converter will have inrush current because of the capacitor inside, the activation time for 3 of them is quite different
- after 50 ms receiving 48V, there is inrush current around 33A
- immediately after receiving 48V, there is inrush current around 25A
- Nothing can be observed for the small DC Converter
My DC converters does not have "Enable" for TPS2492 PG function
My question is, Do I really need TPS2492 in the first place? since the DC converter will only turn on, and the load on the output side of DC converter will not be turned on directly until signal being given to them.
If I do not really need HotSwap Board, what other consideration do I need to take for this connection between the Power Supply (From Battery) to this machine?
I tried to use the calculator with my selection of FET but it seems that my FET spoilt after my first activation
Thank you!