This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3424: setting up parameter

Part Number: LM3424


   i am currently trying to drive 3 series and 10 parallel combination of CREE led at 2.5 amp average led current these led work at 3v forward now i need around 9v at output but my load i.e Rd is 97.5mohm (net resistance of 30 led arrangement ) now i am confused that if lm3424 is trying to control the current only current monitoring how this 9v at output is achieved can someone please explain it because iled *rlednet(.0975*2.5) is not 9v