Other Parts Discussed in Thread: TAS5828M
Hello,
I am using the LM3478 to convert a 2-cell LiPo battery (7.4V nominal) to a dynamic voltage rail for the TAS5828M audio amplifier using its Hybrid PWM Feedback feature to modulate the LM3478 FB pin. I hear audible noise from the boost when this feature is enabled. This led me to investigate my compensation network and I saw that the voltage was not stable during operation. Even in steady-state conditions where the audio amplifier was not modulating the FB pin, the COMP pin goes to its rail every second or so, which corresponds with the timing of clicks I hear. Could I request some help to validate that my compensation is appropriate?
Thanks and regards,
Craig
The image above shows the FB pin on CH1, the COMP pin on CH2, the amplifier Hybrid PWM FB pin on CH3, and the boost output voltage on CH4 while no music is being played.
The image above shows typical behavior of the system while playing audio
In this image, the SW node is shown on CH4 instead of boost output voltage
This shows the output of TI's PurePath Console 3 tool where the Hybrid Feedback feature is configured.
Schematics attached here