This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, all
What is the difference between LP875640RNFRQ1 and LP87564TRNFRQ1? It is not listed in LP8756x datasheet.
Hi Ken,
See the technical reference manuals https://www.ti.com/lit/pdf/snvu815 and https://www.ti.com/lit/pdf/snvu634
Here are the register differences between those two devices.
LP875640RNFRQ1 | LP87564TRNFRQ1 | |||||
Register address | Bitfield name | Value | Value description | Value | Value description | SAME? |
0x01 | OTP_ID | 0x16 | 0x16 | 0x89 | 0x89 | FALSE |
0x02 | BUCK0_FPWM | 0x00 | AUTO mode | 0x01 | Forced PWM | FALSE |
0x03 | SLEW_RATE0 | 0x04 | 3.8 mV/us | 0x05 | 1.9 mV/us | FALSE |
0x04 | BUCK1_FPWM | 0x00 | AUTO mode | 0x01 | Forced PWM | FALSE |
0x05 | SLEW_RATE1 | 0x04 | 3.8 mV/us | 0x05 | 1.9 mV/us | FALSE |
0x06 | EN_BUCK2 | 0x00 | DISABLED | 0x01 | ENABLED | FALSE |
0x06 | EN_PIN_CTRL2 | 0x00 | EN_BUCK2 bit | 0x01 | EN_BUCK1 bit AND ENx pin | FALSE |
0x06 | BUCK2_FPWM | 0x00 | AUTO mode | 0x01 | Forced PWM | FALSE |
0x07 | SLEW_RATE2 | 0x04 | 3.8 mV/us | 0x05 | 1.9 mV/us | FALSE |
0x08 | BUCK3_FPWM | 0x00 | AUTO mode | 0x01 | Forced PWM | FALSE |
0x09 | SLEW_RATE3 | 0x04 | 3.8 mV/us | 0x05 | 1.9 mV/us | FALSE |
0x0A | BUCK0_VSET | 0x0A | 600 mV | 0x61 | 1100 mV | FALSE |
0x0C | BUCK1_VSET | 0x0A | 600 mV | 0x61 | 1100 mV | FALSE |
0x0E | BUCK2_VSET | 0x0A | 600 mV | 0x4D | 1000 mV | FALSE |
0x10 | BUCK3_VSET | 0x0A | 600 mV | 0x61 | 1100 mV | FALSE |
0x21 | TDIE_WARN_MASK | 0x01 | MASKED | 0x00 | UNMASKED | FALSE |
0x22 | RESET_REG_MASK | 0x00 | UNMASKED | 0x01 | MASKED | FALSE |
0x28 | PG3_SEL | 0x01 | Power-Good-threshold voltage | 0x00 | Masked | FALSE |
0x28 | PG1_SEL | 0x01 | Power-Good-threshold voltage | 0x00 | Masked | FALSE |
0x28 | PG0_SEL | 0x01 | Power-Good-threshold voltage | 0x00 | Masked | FALSE |
0x29 | HALF_DELAY | 0x00 | 0-15ms (DOUBLE_DELAY=0) / 0-30ms (DOUBLE_DELAY=1) | 0x01 | 0-4.8ms (DOUBLE_DELAY=0) / 0-9.6ms (DOUBLE_DELAY=1) | FALSE |
0x2C | EN_SPREAD_SPEC | 0x00 | DISABLED | 0x01 | ENABLED | FALSE |
0x2C | GPIO3_SEL | 0x00 | EN3 | 0x01 | GPIO3 | FALSE |
0x2C | GPIO2_SEL | 0x00 | EN2 | 0x01 | GPIO2 | FALSE |
0x2D | GPIO1_OD | 0x01 | Open-drain output | 0x00 | Push-pull output | FALSE |
0x2D | GPIO3_DIR | 0x01 | Output | 0x00 | Input | FALSE |
0x2D | GPIO2_DIR | 0x01 | Output | 0x00 | Input | FALSE |
0x2D | GPIO1_DIR | 0x01 | Output | 0x00 | Input | FALSE |
0x2F | GPIO3_OUT | 0x00 | Logic low level | 0x01 | Logic high level | FALSE |
0x2F | GPIO2_OUT | 0x00 | Logic low level | 0x01 | Logic high level | FALSE |
BR,
Samuli
Hi Ken,
Ah, you are correct. I fixed the table now. The right one is LP87564T-Q1.
BR,
Samuli