Hi team,
I recently purchased the BQ50002AEVM on receiving side we have BQ51013 IC in our PCB and rechargeable battery, while trying to establish the power transfer I am able to observe the all below conditions.
But after placing the receiver LED D6 in the EVM I am not seeing it ON can you please suggest me what is the reason for not going for power transfer phase, necessary steps to be taken
Condition |
Remarks |
I_in_lmt=500mA, V_limit=5V |
D1 ON (Without receiver) |
Input voltage at J1 is 4.9 V to 5.1 V and current is less than 100 mA with a high-to-low fluctuation or |
Observed the same |
2. On UUT PWR607, Power On green LED D1 is ON |
Observed the same |
3. On UUT PWR607 LED D4, D5 and D6 are OFF |
Observed the same |
4. Using current probe, monitor input current and observe digital pin will occur every 5 s for 70ms |
Observed the same |