This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5069: Design Review

Part Number: LM5069

Hello TI Team,

I have designed LM5069 for OV and OC protection for a load supplied from a battery Li Ion.

Could you help me out by reviewing my design

/cfs-file/__key/communityserver-discussions-components-files/196/2021.60C_5F00_temp.xlsx

Also I have 5 questions

1) In the current limiter section what do you mean by minimum, typical, maximum current limit.

2) In startup section the startup time is 114.00 ms but the fault timeout is 0.47 ms. In the video it was mentioned that this would affect the device.

    Could you kindly check the design and let me know if there is a problem

3) What is VDD connected connected to PGD

4) Also what do you mean by upper and lower threshold for UVLO and OVLO

5) I do not know my output load capacitance to accurately enter in operating condition sections, so what would be a good value ?

Thanks