This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6594EVM: does not work

Part Number: TPS6594EVM
Other Parts Discussed in Thread: TPS6594-Q1

We are tried to connect with TPS6594EVM1212EVM via GUI tool, but  there was something wrong with connecting board.   The behavior of power supplies are below,  so please kindly tell us how to recover it ? 

Using the silk for J15 (same as the schematics)
J15 -6 (silk VSYS SENSE) measure 0V
J15 -7 (silk 3.3V) measure 3.3V
J15 -8 (silk VSYS) measure -0.116V
J15 -9 (silk 5V) measure 5V

Using the silk for J30 (same as the schematics), jumper connecting pins 2 and 3
J30-1 (silk 1.8V) measure 1.8V
J30-3 (silk 3.3V) measure 3.3V

TP1 (silk VCCA) 0V
Note board version BMC047A

※ we saw related topic on the forum, but asking just in case.