Other Parts Discussed in Thread: BQ24600
Hi TI Team,
I would greately appriciate if you could give this a look over and give me your opinions on this schematic.
The BMS is designed to work with 6 Li-Ion cells. 4.45 per cell, OC would trip at 10A. LEDs and temperature sensor are externally connected. I don't feel like Pre-discahrge and pre-charge will be needed for this since the capacitive load that the device this bms is designed for won't be greater than 5A. The pre-charge is done by the BQ24600 based charger. (If I undestood that correctly.)
I followed the application design for the development leaving out features I belive aren't nessecary for this BMS. Let me know if I have left out something cruicial.
I'll attach a PDF of the schematic with this post.
Kind regards,
Patryk.