Hi Team,
Previously I have already posted a similar thread to enquire about UCC28061(Thread ID: 1105457). I have decided to open another new thread because there is a few more enquiries from my customers.
Could you guide us on the questions below:
- Why do the two gate outputs work at different frequencies (GDA = 120KHz and GDB = 167.4KHz)?
- Why are the two gates not running 180° out of phase.
- Why are the two gates always turn on at the same time during start up?
- The PFC output can't be regulated at no load. But can be regulated under light load.
- Why are the comp pin unstable at no-load?
- Why the comp pin going high (about 4.9V) for about 400ms after AC off. if ac recycle within 400 mS, then the soft start cannot working.
- How Soft Start Works
- How to set the maximum on duration(Ton-max)?
- How to set the maximum and minimum operating frequency?
Attached is the waveforms for reference.
Thank you very much for your constant support!
Best Regards,
Ernest