This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610EVM-532: BQ28Z610EVM-532 can support 2S battery Pack ..?

Part Number: BQ28Z610EVM-532
Other Parts Discussed in Thread: BQ28Z610, BQ34Z100, BQSTUDIO

Hello TI, 

I am using UB26650-7.2V-5000mAh battery pack, which have Inbuilt Short circuit protection circuit, it has two 26650 cell  which connected in series and i have only 2 battery connection which is Pack+ and Pack-.

Battery Pack,

Nominal voltage- 7.4V 

Charging voltage- 8.4V

Capacity- 5000mAh 

BQ28Z610EVM-532 can support UB26650 battery, if yes, guide us how need to interface with BQ28Z610EVM..?

Thanks, 

Rahul