Part Number: LM2576
Hai Sir,
Based on Customer recommendation we are using LM2576-5.5 for voltage conversion.
End application- Controlling & Analog outputs driving.
Can you please give me the clarification about my queries posted below...
1) Designing Vin= 12V to 36V and Vout= 5V, Iout= 1.5A to 2A (Step down conversion)
-> As per the Datasheet reference 8.2.1 Fixed Output Voltage Version , page no.19. Downloaded the Pspice model from TI, Simulated and Verified the Results as per the design.
-> Here external components used Cin- 100uF, Cout- 1000uF . Can we use these capacitor values with Ceramic capacitors and is there any extra smaller capacitors required with these bulk values.
-> Inductor used L-100uH, can we use this value for Iout-1.5A to 2A ?
-> Is it required heat sink for this device with Vin-12-36V, Vout- 5V @ 1.5A, Ambient temp- 50°C
-> Please clarify above mentioned queries