This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC24612: MOS driver issue

Part Number: UCC24612


Hi Team

Currently using 24612 on the new board, there is a problem: Gate cannot be opened normally as shown in the figure below (load0.5A-5A cannot be used)
Using UCC24612-1EVM on customer board can be opened normally, but after replacing the MOS of UCC24612-1EVM, it cannot be opened normally


Does this IC have special requirements for MOS? Is it possible to adjust the peripheral parameters to improve this phenomenon?
*REG measurement is normal
*VCC measurement is normal