Hello. I'm making a 150W converter using the UCC256303. One problem I'm having right now is that the switching frequency doesn't seem to be stable. It's "jittering" when I look at the oscilloscope, and the transformer is making a lot of noise because of it, I think.
Do you know any reasons why the switching would be unstable? I'm including a short video of the "jittering" going on, measured on the secondary side of the transformer. Hope its possible to see it