Hi,
In lm5303 Datasheet, Section 8.2.2.3, for finding Cd equation, What is the meaning of term " Lp_used ". Is the value that should be used here is Lp?
For the exampe give in datasheet Lp=400uH
Jacob
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In lm5303 Datasheet, Section 8.2.2.3, for finding Cd equation, What is the meaning of term " Lp_used ". Is the value that should be used here is Lp?
For the exampe give in datasheet Lp=400uH
Jacob
Hello Jacob,
I believe that the term "Lp_used" is derived from the distinction made between "Cd" and Cd_used" in the text following equation (54).
The author probably did not realize (at the time) that this inconsistency is the only instance of "Lp_used" throughout the datasheet.
Note that equation (53) relates t_dlyqr to RFF x Cd, so of course, Cd = t_dlyqr/RFF.
Also, equation (52) equates t_dlyqr to an expression containing "Lp", and this expression is substituted in for t_dlyqr in equation (54).
So, Lp_used is the exactly same as Lp, and I think "Lp_used" was inadvertently coined while the datasheet author was drawing a distinction between the overall Cd needed for timing and the external value required (Cd_used) when accounting for the already-present 20-pF pin capacitance.
Please simply consider "Lp_used" to be identical to "Lp".
Regards,
Ulrich