Part Number: BQ78350-R2-DEVICE-FW
Hello,
In the technical reference document of BQ78350-R1A, it is stated that the ChargingStatus() command returns two byes as follows:
However, after updating my device to the BQ78350-R2 firmware, I saw only one bye in the BQSTUDIO app:
Does it mean that the second byte is removed in the newer version? Then, how is it possible to check if pre-charging conditions or fast-charging conditions are met? Previously, we could check that by the [PCHG] and [FCHG] bits in the ChargingStatus() command.
Sincerely yours,
Shayan