This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Hard Reset issue

Part Number: BQ76952
Other Parts Discussed in Thread: BQSTUDIO

Hello Team,

Hard Reset of BMS IC through Switch S2 is not happening, but when I connect to BQSTUDIO software and reset it through command, Reset is happening fine. What am I missing here?

Thank you

  • Hi Mohammed, 

    Performing a reset through the pin doesn't reset the registers because it's a partial reset.  A full reset can be accomplished through issuing the RESET command, as you have already observed.  You should also note that the partial reset will not be performed through the pin if Reg1 isn't powered on as there will be no voltage.

    Best,

    Andria

  • Hi Andria,

    In the attached image, I have given 3.3V from an external source as I am not be using Reg1 and Reg2 internal LDOs. I have noticed that partial reset is also not happening with the current circumstances. Is there a workaround to this. I need a hard reset circuitry to reset the BMS IC.

  • Hi Mohammed,

    Unfortunately, you will not be able to perform a hard reset using the RST_SHUT pin or external circuitry.  A hard reset can only be performed by issuing the RESET command.  If you are willing to put your device in shutdown mode, you can shut down and then wake up your device to reset the register values, if resetting register values is your main concern.  To accomplish this, please refer to section 7.5 SHUTDOWN Mode in the TRM.  I will attach a link here: BQ76952 Technical Reference Manual (Rev. B) (ti.com).

    Best,

    Andria

  • Hi Andria,

    Thanks for the clear response.

    Can I do the partial reset as explained in the TRM with the current setup (Refer the image attached above)?

  • Hi Mohammed,

    You should be able to perform a partial reset by raising the RST_SHUT pin high for < 1 second.  Your button configuration shown in the schematic you attached should allow this.  I would recommend double checking to ensure that the 3.3 V you have from an external source is in fact supplying voltage to the RESET section of your schematic if you are not able to perform a partial reset via the RST_SHUT pin.

    Additionally, the effects of a partial reset are subtle, so please refer to this thread to tell if a partial reset has occurred: BQ76952: Accumulated charge returns -32768 - Power management forum - Power management - TI E2E support forums.

    Best,

    Andria