Hello TI,
Currently I'm testing TPS6281120QWRWYRQ1, when i test for current that flowing through inductor with the following conditions
Vin = 6V DC (keysight E36231A)
Load current - 265mA (scientfic SME1701)
Inductor peak current(I_L max) is going to 818.3mA
I_L min is going to -274.4mA
1)Since the convertor is operating in CCM mode why the inductor current is going to negative
2) why the ripple current is very high (delta I_L ) that is 1.0927A,Could you please help me on these two