This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6594-Q1: how to realize cold start

Part Number: TPS6594-Q1
Other Parts Discussed in Thread: DRA821, TPS6594EVM

Hi Expert,

Our customer use TPS6594-Q1 power DRA821.

They want to realize cold start function via nRSTOUT pin. During the cold start, all TPS6594-Q1 remains unchanged, meaning the output all on. DRA821 config TPS65941 via i2c to pull low nRSTOUT to reset DRA821. But the nRSTOUT  will automatically pull high after certain time. There is no other external SoC will pull nRSTOUT high since it is not running. nRSTOUT is required to pull high automatically. This function is similar with ESM_ERROR but they don't want to use it since it will leave some fault counter. So is it possible to achieve this function? Thanks.

BR,

Elec Cheng