This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61230: Using two in parallel

Part Number: TPS61230


Does this boost regulator support using 2 in parallel?  I know that not all boost devices can support parallelization, but I found this thread showing that the part in question does support parallel use:

e2e.ti.com/.../tps61288-using-two-in-parallel

There is even a reference design for the device discussed in that thread: www.ti.com/.../PMP40909

Also, if TPS61230 supports using 2 in parallel, what is the maximum continuous output current I could expect to source from the parallel combination of two of those devices?

Thanks in advance,

Paul