Hello,
We are considering using your PTH08080W module to power the Iridium 9602 satellite transciever. The power supply requirements for the Iridiums are:
(11 to 15 VDC Input, 5VDC 2A output)
1) Droop for 8.3ms burst of 1.5A current should not be more than 0.2Volts.
2) In-rush current to Iridium limited to 4A maximum.
Will this module do the job? Can you recommend this part or is there another that might be better? This is a battery operated system so efficiency is important.
Thanks.
Loren