This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750EVM: Error reprogramming EVM

Part Number: TPS25750EVM
Other Parts Discussed in Thread: TPS25750

I'm using the TPS25750EVM to test a poc bi-directional battery charging circuit. For testing purposes I configured it as a 5V 3A power source only, which worked as expected. Now when I try to upload a new configuration, I get the error message "An error occurred while flashing to device. Try power cycling EVM and reconnecting hardware before flashing again."

I've rebooted it several times and I keep getting the same error. Is there a way to reset it so I can flash a new configuration?