Dear team,
Can you help us clarify questions?
How to fully use 12-bits resolution of PWM in LP5024?
But, the registers are 8-bits only.
From the datasheet, it says


Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
Because our oscillator fre is 15MHz, so it seems impossible to achieve 29kHz PWM, but our LP5024 has a Built-in algorithm, which can modify the 8 bits color mixing and 8 bits brightness control value to a 12 bits control signal and achieve 29kHz PWM effect.