Hello,
I am trying to simulate the TPS7H5001-SP in PSPICE for TI; however, I am getting an error saying that the subcircuit for the device is undefined. I also receive a similar error with some third part components that I've imported. Any assistance is greatly appreciated.
ERROR:
Reading and checking circuit
ERROR(ORPSIM-16363): Command invalid in subcircuit
ERROR(ORPSIM-16499): Missing .ENDS in .SUBCKT
ERROR(ORPSIM-15460): Subcircuit TPS7H5001-SP_TRANS is undefined
ERROR(ORPSIM-15460): Subcircuit UsersabelfieldDownloadsisl7x040seh-pspice-modelisl70040seh_061818_enc.lib is undefined
ERROR(ORPSIM-15460): Subcircuit UsersabelfieldDownloadsisl7x040seh-pspice-modelisl70040seh_061818_enc.lib is undefined
Circuit has errors ... run aborted
See output file for details
INFO(ORPROBE-3188): Simulation aborted