I am currently working on implementing patching for TPS25750.
Reading Table 3-9 in the TRM, I can see this:
Which is clearly somewhat self-contradictory.
- Is the bundle size meant to be on bytes 0-3, or bytes 1-4?
- Is the byte not mentioned reserved?
- Are the byte numbers above the size correct, or shifted by 1?
While I'm here, let me add that the manual could use a general description of how to use 4CC commands as a second-level section, not buried as part of "3.3.4 Patch Burst Mode Example".