This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
Good morning. We wish to revisit into our power design with this requirement –
Vin = 7V to 15V
Vout = 0.72V
Iout = 9.0A
Ripple < 10mVpp
Power efficiency >85%
Do you have any recommendations that I could further check on? I have shortlisted quite a number of these a year back, but a lot of them has the Vin(max)=16V. We have concern on this as our adapter input is 15V ±3%. (max 15.45V). Do you think this would be a valid concern with the consideration of Vin p-p?
Many thanks.
KLP
I would recommend the TPS543B22. It will release in December, the product folder is located here https://www.ti.com/product/TPS543B22
The input ripple requirement can be meet with additional capacitors or a ferrite bead on input.
The efficiency is greater than 85% at 9A with 12V input at 1000kHz switching frequency.
Using the 750kHz or 500kHz switching frequency, the efficiency will greater than graph below.