Other Parts Discussed in Thread: TPS51650
Hello,
Greetings of the day!TPS59650RSLT.pdfTPS51650 Calculator DCR Sense_10kNTC QC_Aug1_2011_01_Nov22.xls
I am working on Power Section Design of Intel Atom E3826 using discrete IC's & Components (without PMIC). In the design, two core supplies are required for Atom as follows-
CORE_VCC: 4A @ 1.0V
UNCORE_VNN_S3: 10A @ 1.0V.
For the above requirement, I am using TPS59650RSLT from TI. This component has 3 CPU phases & 2 GPU phases. And, I have used 1 CPU (for CORE_VCC) & 1 GPU (for UNCORE_VNN). Kindly preview the attached schematic for the reference.
Now, My doubts are-
1) As I am Not using 2 CPU & 1 GPU phases, what should I do with their unused respective pins?
2) Are Bulk capacitors required for the output current 10A & 4A.
3) As I am following Spreadsheet "TPS51650 Calculator DCR Sense_10kNTC QC_Aug1_2011" for the reference, what Inputs should I take for the following sections-
3.A) Thermal Design Current (I_TDC_total)?
3.B) value of B value of DCR thermal compensation NTC and Resistance of NTC at 25C ?
3.C) what is meaning of OSR/USR setting level at COCP-R and GOCP-R that is fixed at 1V & 1.6V?
3.D) IMON voltage at Icc_max?
Please help preview the attached schematic & Design Spreadsheet for the reference-
As, We have on-board space constraint, so please consider use of optimal components while reviewing the design.
Thanks & Regards
Raj Kumar