Dear Expert,
The attachment is our test data, if you have a few questions, please help to answer, thank you!
1. There is no label on the Vds transient negative pressure manual. Does our waveform meet the specifications?
2. After the DRMOS input 0402 filter capacitor is removed, the Vds has little effect. After removing a 22uF capacitor, the Vds increases significantly, but it still does not exceed the specification of 20V.
3. When the 1-phase output is changed to two-phase output, the HS Vds generally decreases, but the LS Vds increases. Please help explain the reason and assess the risk, thank you!
test method:
Schematic:
Many Thanks,
Jimmy