Hello Sir:
Please help to check our schematic.
We want to use BQ76952/42 in the same schematic.
If there has any thing wrong please kindly let us know.
Thanks a lot.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Sir:
Please help to check our schematic.
We want to use BQ76952/42 in the same schematic.
If there has any thing wrong please kindly let us know.
Thanks a lot.
Hi Statham,
Yes, this should work.
I notice the capacitors on the thermistor pins are larger than recommended in section 16.2 of the datasheet. The TI Reference designs use 470pF for these pins. Also, the TS2 pin is the wake pin for the device, so it is better not to connect a thermistor to this pin if the Shutdown feature will be used. Other pins like DDSG and DCHG can be used with thermistors instead.
Best regards,
Matt